New OLFLEX® Servo FD 796 CP

Seven in One
The new ÖLFLEX® SERVO FD 796 CP motor cable is being launched with the tag line "Seven in One". The new premium cable can replace seven of our existing servo motor cables at once, offering users a whole range of additional benefits.
The operation of automated machinery requires many positional changes and variants in speed, this is where the new premium cable from Lapp shows its excellence. With an acceleration of up to 50 m/s² and speeds of up to 5 m/s and travel distances up to 100 m the new ÖLFLEX® SERVO FD 796 CP offers a significantly faster and more efficient operation than previous servo chain cables.
The proportional run-up and braking times have also been reduced by up to 96%. Due to the low capacitance polyolefin insulation it offers lower EM-effective leakage currents while simultaneously providing extremely high dielectric and electrical strength. It is halogen free and flame retardant and has the key approvals in UL & CSA.
The new servo motor cable offers an exceptionally long service life, is compact and lightweight.
See the full range of the ÖLFLEX® SERVO FD 796 CP